NEWS
 

STMicroelectronics Boosts MEMS Portfolio with New ‘Gyroscope’ Angular Rate Sensors Offering Extended Supply Voltage Range

Miniature, surface-mountable gyro sensor offers extended power supply range, power-management capabilities, high stability, excellent shock resistance, and 300 degrees-per-second angular rate measurement

Click for larger image Geneva, June 09,2008 - STMicroelectronics (NYSE: STM), a market leader in MEMS products, has introduced the LISY300AL, a 7 x 7 x 1.5mm surface-mount MEMS single-axis yaw gyroscope for angular rate sensing up to 300 degrees per second (full scale). The new device combines high sensitivity, an extended supply voltage range, from 2.7V to 3.6V, and a selectable power-down mode. It also provides reduced standby power for applications such as game controllers, intuitive pointers, vehicle or personal navigation, and image stabilization.

Drawing on the company’s market-leading expertise in MEMS, and combined with highly robust MEMS technology, the LISY300AL exhibits stable sensitivity and bias-voltage throughout variations in temperature and over the device’s lifetime. This simplifies design and promotes reliable operation. Also featuring a co-integrated low-pass filter and dedicated IC interface, the LISY300AL enables a compact, low-noise solution using minimal external components. In addition, high survivability of shock and vibration allows use in demanding environments including industrial and automotive systems. An embedded self-test function provides extra assurance of accuracy and reliability.

In addition to consumer and industrial applications, including gaming and smart user interfaces for advanced pointing devices, the LISY300AL can be used for tilting and angular motion detection in robotics and assisted-GPS navigation systems.

The LISY300AL generates an absolute-rate output as an analog voltage. The 28-lead LGA device uses ST’s ECOPACK® packaging, which meets ‘green’ criteria for RoHS compliance.

Samples of the LISY300AL are available immediately, with production volumes scheduled for introduction in Q3 2008 at prices from $2.50.

Further information is available at:
http://www.st.com/stonline/products/families/sensors/gyroscopes.htm

Click here for the high-resolution photo


About STMicroelectronics
STMicroelectronics is a global leader in developing and delivering semiconductor solutions across the spectrum of microelectronics applications. An unrivalled combination of silicon and system expertise, manufacturing strength, Intellectual Property (IP) portfolio and strategic partners positions the Company at the forefront of System-on-Chip (SoC) technology and its products play a key role in enabling today's convergence markets. The Company's shares are traded on the New York Stock Exchange, on Euronext Paris and on the Milan Stock Exchange. In 2007, the Company's net revenues were $10.0 billion. Further information on ST can be found at www.st.com.
Information last updated Jan 2008





Should you require more information, please select the appropriate contact from the "Related Topics" menu.