High-density ST23YL secure ICs are industry’s first smartcard controllers certified to EAL 5+, according to latest Common Criteria version 3.1
|
Geneva,
October 31,2008 -
Two smartcard controllers from STMicroelectronics (NYSE: STM), a world leader in smartcard ICs, have become the industry’s first devices certified to Evaluation Assurance Level 5+ (EAL 5+) of CC v3.1, the latest revision of the ISO/IEC 15408 Common Criteria for IT security products.
The ST23YL80 and ST23YL18 secure ICs have been designed to support highly secure applications such as PayTV, ID cards, IT security and Payment. The ST23YL platform features a 8/16-bit secure processor, secure non-volatile memory, and a cryptographic co-processor (Nescrypt) supporting fast and secure public key algorithms such as RSA and Elliptic Curves. The devices are built using ST’s 0.13-micron EEPROM process, resulting in small chip size, low power consumption, and consistently high quality.
Common Criteria v3.1, the latest version of the Common Criteria, enables widespread mutual recognition of secure IT products used by commercial organizations and government bodies globally. EAL 5+ is the highest achieved assurance level for commercial products, and allows the ST23YL controllers to be used directly in smartcards for highly secure applications with no further reassessment or acceptance testing required. In addition, for Payment systems, the ST23YL Secure ICs are also certified by EMVCo and have been recently assessed as suitable for the German market by ZKA authorities.
ST is a leading advocate for formal security evaluation of smartcard controllers to international standards. In 2000, it became the first company to achieve CC certification for a smartcard IC, when its ST19 microcontroller was certified to CC EAL 4 Augmented, and has consistently certified its products to the highest assurance levels for commercial applications.
Click here for the high-resolution photo
About STMicroelectronics
STMicroelectronics is a global leader in developing and delivering
semiconductor solutions across the spectrum of microelectronics
applications. An unrivalled combination of silicon and system
expertise, manufacturing strength, Intellectual Property (IP)
portfolio and strategic partners positions the Company at the
forefront of System-on-Chip (SoC) technology and its products play a
key role in enabling today's convergence markets. The Company's
shares are traded on the New York Stock Exchange, on Euronext Paris
and on the Milan Stock Exchange. In 2007, the Company's net revenues
were $10.0 billion. Further information on ST can be found at www.st.com.
Information last updated Jan 2008
|
|
|
|